10/4/2018 2:28 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, there is no difference between D410-2 and CU310-2 on drive side concerning drive commissioning. You can do a new commissioning. 4.14 Motor data identification https://support.industry.siemens.com/cs/ww/en/view/109757573 You can check the pole angle The pole position identification is used for: ●Determining the pole position (p1982 = 1) ●Determining the commutation angle offset during commissioning (p1990 = 1) ●Plausibility check for encoders with absolute information (p1982 = 2) You can move encoderless for a test, to check the encoder signals. Operation without an encoder is activated using parameter setting p1300 = 20. |
With best regards, |
|
Follow us on