6/25/2013 11:55 PM | |
Joined: 1/30/2009 Last visit: 8/12/2025 Posts: 18 Rating:
|
Graeme What is IVI and PSU cards? How can I diagnose these after CUVC board? |
6/26/2013 5:37 AM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
IVI is interfacing card - this card is used for interfacing control cicuit and power circuit PSU - is power card - this card gives power supply required by control circuit (24V) You can read more detailed description of hardware basics of master drive from following thread /tf/WW/en/Posts/21854 - And regarding your doubt about CU faulty or not - for that you can just try swapping CUVC from faulty drive to healthy - if fault is also swapped than CUVC faulty otherwise you need to check further Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/4/2013 11:06 PM | |
Joined: 1/30/2009 Last visit: 8/12/2025 Posts: 18 Rating:
|
How do i find out if U950,U951.....blocks are being used or not? |
9/10/2020 2:15 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by Saadi1981 is split to a separate thread with the subject Simovert fault message: Measuring Value Sensing. Best regards |
Follow us on