8/25/2008 6:30 PM | |
Posts: 15 Rating:
|
You can use an input (F key or hardware input) and increment a shift register. The logic state of the shift register can be used to enable an array of "AND" gates that control message text. Each instance of the message text can be unique. With the new version of the software, you and use the status of the inputs or outputs to change the text displayed on any given message. I will be using this arrangement for one of my applications. I hope this helps.
AttachmentNew Logo F Key control example.zip (1375 Downloads) |
Last edited by: FogBot at: 8/25/2008 6:59 PMAdded attachment |
|
8/25/2008 9:26 PM | |
Posts: 10 Rating:
|
Thanks Fogbot for that... I will try to advance with this.. I will give a feedback asap.. Regards |
8/27/2008 3:17 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi, at the german part of this forum you can find some examples from me, how to manage menues with the new LOGO!-series 0BA6: "Logo0BA6 + TD und Menüsteuerung" (attachment direct: Demo_TD_Menüs.zip) best regards Betel |
==> Meine TAG-Listen: "deut." |
|
8/27/2008 4:57 PM | |
Posts: 191 Rating:
|
hi!! this is another program that could give you some ideas hope it helps!! ROSA Attachmentmenu.zip (1337 Downloads) |
8/31/2008 9:31 AM | |
Posts: 10 Rating:
|
Ok, attached my actual rush... What i need to replace is all temp input system, because i will use AM2 PT100 module instead 0-10v analog input asactually in the file.I began my draw from this point, reading a post "about filters"..... For this last point, i have a doubgt and i will open another post not to mix all in one... The other point, i want to display in which timming step the system is running and have the possibility trough the display and keys to force the timming step manually for a period of 24h then the system will be back to original automatic running process. That's the reason why i need "menus" and "submenus" and "commands"from the logo display and arrow keys. Please give me your comments. Regards, Henri Attachmentpoll rush OBA5 beta1.zip (1110 Downloads) |
8/31/2008 5:46 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi riiri7707, "The other point, i want to display in which timming step the system is running and have the possibility trough the display and keys to force the timming step manually for a period of 24h then the system will be back to original automatic running process." First i think, that the arrow-keys are not the best solution if you use the new external TD, because to use an arrow-key you must holt the [ESC]-key at the same time too.... To answer at your question please tell me/us more (all) details for the programmed function you want and the corresponeded user action(s) (text and/or pic) for better understand and a "special" solution for your aims! Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
8/31/2008 6:48 PM | |
Posts: 10 Rating:
|
Thanks Betel, Attachmentpoll rush OBA5 PT100 beta2.zip (1063 Downloads) |