3/16/2022 1:12 PM | |
Joined: 1/18/2021 Last visit: 8/3/2023 Posts: 31 Rating:
|
Sinamics S120 Tia Portal V16 with Startdrive |
Last edited by: Joanna.S at: 03/16/2022 13:14:09 |
|
3/17/2022 9:54 AM | |
Joined: 1/18/2021 Last visit: 8/3/2023 Posts: 31 Rating:
|
Thank you a lot! I think something is missing in the configuration for sure ;( I am now reading the instruction: S7-1500/S7-1500T Motion Control overview V5.0 in TIA Portal V16 (siemens.com) and it says to drag and drop telegram from the hardware config to the device view of CU. I have chosen telegram 105 and configured it in the properties -> telegram configuration of the CU. I tried to see if I can telegram from the hardware but I cannot drag anything to the device view (I used devices detection for hardware configuration) Should I use isochronous mode for both CU + motors? Attachments71500_s71500t_motion_control_overview_function_manual_en-US_en-US.pdf (767 Downloads) |
Last edited by: Jen_Moderator at: 03/17/2022 12:27:25Added PDF as an attachment. |
|
3/17/2022 10:59 AM | |
Joined: 1/18/2021 Last visit: 8/3/2023 Posts: 31 Rating:
|
I am sorry but how can I add the TIA portal project here? i got compress file Zap16 but this is not acceptable here? |
3/17/2022 11:10 AM | |
Joined: 4/28/2015 Last visit: 9/11/2025 Posts: 1278 Rating:
|
Just zip the project file |
Best regards, |
|