6/3/2016 11:10 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, How or where from you derived mentioned encoder details? If the encoder details A32S/R you provided assumed to be correct, then motor MLFB number would be 1KF7063-5AF71-1GB3 & not 1KB3. This motor is without Drive-CLiQ encoder interface. 1KF7063-5AF71-1KB3 motor is with Drive-CLiQ encoder interface & encoder is 16 bit absolute encoder single-turn +12 bit multi-turn. So both motors encoders are not equivalent & I am surprised as how you connect or replace it. Please refer attached sheet for more information. HTH. Attachment1FK70 motor MLFB .pdf (735 Downloads) |
6/15/2016 8:36 AM | |
Posts: 7 Rating:
|
Both motor have one power connector with big pins and one RJ-45 looking connector.... . |
6/28/2016 11:25 AM | |
Posts: 7 Rating:
|
here is the photo from the motor name plate. ....1KB3 and I have AM32 S/R encoder not AM16DQ as the K indicates in the catalog.... |
Follow us on