1/2/2015 9:43 AM | |
Posts: 784 Rating:
|
|
1/18/2016 9:28 PM | |
Posts: 1 Rating:
|
its not the basic software , its just an update for the basic software,,, waste of time.. |
3/20/2016 8:11 PM | |
Posts: 1 Rating:
|
When I start to install it, it says it is the version 1, isn't it supossed to be the 4? Thanks |
3/21/2016 7:25 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, pls why you don't look at dokumentation files for instalation? There must be info about version. |
With best regards... |
|
4/12/2016 8:56 AM |
|
Joined: 7/1/2014 Last visit: 5/7/2025 Posts: 237 Rating:
|
Thanks for the link! :) |
4/12/2016 11:12 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, MICROWIN is not a free ware. And the provided links in the start of this thread was for only service packs. And also it's indicated clearly inside the link that it doesn't containing the basic software. Software Part number is: 6ES7810-2CC03-0YX0 But please note that announcement for this product to be phased out is dated 1/11/2015 Which means that it will be cancelled soon. Hope this helps. |
Ayman Elotaify |
|
6/27/2016 9:49 AM | |
Posts: 4 Rating:
|
Hello Sirs, I am just a new born in PLC world .i have CPU315-2DP with me and i have step7 microwin v4.0 sp8 , are the hardware and software compatible or shoud I download a specific Sp version so that I can write program to my PLC? thanks in advance for your answer |
6/27/2016 11:33 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, no, your CPU isn't compatible with that SW - MicroWin. MicroWin SW is prepared for lower type CPUs - S7-200. Look for Step7 v5.5 or TIA Portal versions, they are prepared for S7-300 CPUs. Also use of Step7 v5.5 or TIA Portal depends on type and firmware of S7-300 CPUs, so old versions of S7-300 CPUs can be programmed only with Step7 v5.5 and newer versions on both SW - Step7 v5.5 and TIA Portal. So look to your CPU exact number and firmware version, but better will be contact your local Siemens representative to obtain all needed infos about products and prices. |
With best regards... |
|
This contribution was helpful to
2 thankful Users |
7/10/2016 2:30 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, As Duris told, you have to go to Step 7 (Clasical type: V5.5) or TIA type. You will spend some money to buy this software package. But as you are new born in PLC and if you have only a central rack (I am not sure if that's your case or not), you can use STEP7 Lite! It's a free ware and cn be download from the following link: STEP 7 Lite V3.0 incl. SP4 Available for Downloading Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
Follow us on