2/29/2024 11:32 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
there is no update afaik. which error exactly you get? |
This contribution was helpful to
1 thankful Users |
3/1/2024 10:50 AM | |
Joined: 8/3/2009 Last visit: 9/11/2025 Posts: 16400 Rating:
|
Hello Roby There is something wrong with your filesizes of the Image download files, check the screenshot you have posted again and compare it to the sizes that are written in the download FAQ. It seems that the .001 file is not correct... perhaps you have downloaded the wrong one.. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
3/1/2024 12:13 PM | |
Joined: 4/10/2006 Last visit: 9/8/2025 Posts: 963 Rating:
|
********** SOLVED ********** For versions higher than TIA V17 it is necessary to update the firmware to the TP1500 by downloading this version: from this link: Panel images ATTENTION: do not unpack any files but put them all in a folder and run the executable. Many thanks to everyone involved in this post Roby |
Setting of my PG M6 Siemens |
|
This contribution was helpful to
1 thankful Users |