11/14/2023 7:32 PM | |
Joined: 8/28/2023 Last visit: 12/5/2024 Posts: 12 Rating:
|
A different inverter with another problem. Installed a new inverter , Siemens V20 , 11 kw to a benchsaw which , in the past had many problems with the mechanical brake. It was decided to replace the star delta setup with an inverter. Ordered the V20 11KW inverter after seeking advice from the supplier. With all Parameters for the motor set as shown below , following a factory reset. Volts – 400 HZ – 50 RPM – 2910 PF – 0.82 Amps – 17.8 KW - 9.25 Min Frequency – 50Hz Max Frequency – 50 Hz Acceleration Time 10 Secs Deceleration Time 10 Secs. When trying it today I had the following error Accelerates OK Deceleration – Alarm Code A911 Shows on display , initially braking then freewheeling to a stop. VDC_max controller active. First two times I started and stopped the motor , deceleration was ok. I would appreciate some advice please. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2023 09:41:54New subject after splitting |
|
1/17/2024 6:04 PM | |
Joined: 8/28/2023 Last visit: 12/5/2024 Posts: 12 Rating:
|
Thanks for your advice , I will look around for a suitable enclosure |
Follow us on