(3)| 2/12/2021 6:50 PM | |
|
Posts: 8 Rating:
|
Hello, It's an extrusion line, the motor 6 is the Winder and motor 1 is the Conveyor Belt,. In PLC program the OB34 (Extrusion Program) has the maximum speed/maximum production speed/ Reference speed, I understand that I should try to change something here. I've tried to change all theses speeds to 50m/min instead 1000m/min expecting that it was limiteded, but nothing happened. In Winder program and S120 the limit is 1200m/s. I will attach two pictures here, Dryer is the previous station before Winder. Please take a look if it is possible, I use profinet communication, all the motors works with feedback encoder active, I will check if We use analog control... I really appreciate the support on this post. Thanks all! Igor AttachmentOB34-Extrusion.pdf (299 Downloads) |
Follow us on