(0)| 12/24/2008 6:50 AM | |
|
Joined: 9/27/2006 Last visit: 1/14/2026 Posts: 12481 Rating:
|
Hello Nevaland; Look at the following attachments, they are extracted from the manual "Bus Links: DP/PA link and Y-link". The first one shows the architecture schematic, as requested. The second one shows the required hardware to build a Y-Link. The Y-link is a master on the downstrean Profibus side, and is strictly limited to 244 Bytes IN/244 Bytes OUT; check out the data from the manual, you should understand it well before you start designinig your project. The complete manual can be found here: http://support.automation.siemens.com/WW/view/en/1142696 Hope this helps, Daniel Chartier |
| 2/19/2009 10:47 AM | |
|
Posts: 12 Rating:
|
hi Mr.dchartier, i think the following link may be useful for Mr.Nivaland. http://support.automation.siemens.com/WW/skm/frameset.asp?url=%2FWW%2Fllisapi%2Edll%2F19951154%3Ffunc%3Dll%26objId%3D19951154%26objaction%3Dcsopen%26skm%3D1%26lang%3Den&Query=master+slave+configuration+with+Y%2Dlink+&SearchArea=alle&id=19951154&F11Marker=true&siteid=cseus&query2=&modelled=&lang=en regards, senthilkumar M. |
Last edited by: CS Moderator at: 2/22/2009 9:13 PMLast edited by: CS Moderator at: 2/22/2009 9:12 PMnew question splitted to a new thread Last edited by: senthilkumar at: 2/19/2009 10:49 AM |
|
This contribution was helpful to
|
|
Follow us on