(0)| 8/31/2021 11:16 AM | |
|
Joined: 1/9/2019 Last visit: 3/22/2025 Posts: 88 Rating:
|
thankyou ChristophD. I want to upgrade the system, the old system uses SIMOVERT MASTERDRIVE VC, I want to upgrade some of them to SINAMICS S120, I think the filter that the old system used is 6ES7023-4ES87-0FB1. should I change the filter and do I need interface module or line reactor? or I can use the old filter instead or I have 6SL3000-0CE23-0AA0 (line reactor for smart line module of simodrive 611) can I use that instead of active interface module? ------------------------------------------------------------------------------------------ |
Last edited by: mpakravanan at: 08/31/2021 13:07:31Last edited by: mpakravanan at: 08/31/2021 13:08:43Last edited by: The Helping Hand at: 09/01/2021 09:16:36New subject after splitting |
|
| 9/1/2021 9:18 AM | |
|
Joined: 8/21/2014 Last visit: 12/19/2025 Posts: 1098 Rating:
|
Closed cause question posted twice. The second thread with the subject using SIMODRIVE line reactor for for s120 active line module is published within the conference SINAMICS S Best regards, |
|
My Forum is the place to personalize your profile, |
|
Follow us on