9/12/2021 9:03 PM | |
Joined: 12/18/2014 Last visit: 9/12/2025 Posts: 35955 Rating:
|
You explain your problem too broadly. Which website are you talking about? How is your signal? |
9/14/2021 7:26 AM | |
Joined: 5/19/2021 Last visit: 11/11/2024 Posts: 27 Rating:
|
thank you for your answers. I'm sorry for the description of the problem. My English is very bad. also, I send you an example file of what I did. The user can put a selector button to put a pump in automatic mode. if there is a power cut, this selector returns to 0.... And the process don t resart . many thanks Attachmentretentivitybit.zip (336 Downloads) |
9/14/2021 8:01 AM | |
Joined: 12/18/2014 Last visit: 9/12/2025 Posts: 35955 Rating:
|
Hello PaulFaud, the problem is that the VM area has no retentivity. In attachment a possible solution. I added a push button with transparent images for On and Off and give them the address V101.5. Then I place the push button over the switch button (same coordinates). The switch button has now the address M1. In the LOGO! program I toogle a pulse relay (B001). By this block you set the retentivity. The output of B001 is connected to the flag M1. Attachmentretentivitybit_V2.zip (337 Downloads) |
Follow us on