(0)| 9/27/2021 12:12 PM | |
|
Joined: 4/28/2015 Last visit: 12/1/2023 Posts: 23 Rating:
|
Hello everybody, I have the same problem, moving files from SD to USB on TP700 Comfort Panel via VB Script. Until I have HW already, I do not know, if there is missing something in the script and if this will even works corectly. For example "reset bit" at the end of the script if should or should not be in the script as a "SmartTag" and for what? Thank you! The body of the script: Sub COPY() Dim fs, fsw, s, s1, d1, src_path, dest_path, wait, fso, folderName ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/27/2021 13:18:22New subject after splitting |
|
Follow us on