12/25/2021 1:39 PM | |
Joined: 8/26/2020 Last visit: 11/17/2024 Posts: 6 Rating:
|
Hello, I am really thankful for your recent answers, helped a lot. There is another thing I wanted to ask about downloading/saving/cloning parameters from an existing operational drive with the help of the Basic Operator Panel (BOP) to a newly installed drive. This is Micromaster 440 drive. Thank you. Kind regards, Irfan ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/27/2021 08:49:21New subject after splitting |
|
12/25/2021 2:58 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello Irfan; You cannot use a BOP to uplaod/transfer a parameter set for a MM440 drive; you need an AOP (Advanced Operator Panel) to do so. This is confirmed by member KonradD in this discussion: - How to download the inverter parameters of MM440 to BOP Details on how the AOP can be used for parameter transfer are descrived here: - MICROMASTER 4 (MM4): Reading a parameter set from an AOP https://support.industry.siemens.com/cs/ww/en/view/9945850 Hope this helps, Daniel Chartier |
Follow us on