3/16/2009 12:32 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Scaras, Look at How do you configure a PC station as DP master for connecting to a DP slave for the SIMATIC NET OPC server with the SIMATIC NET PC software? In this way you can connect Digitric 500 like slave. Of course you'll need GSD file. About WinCC Flex and OPC look at SIMATIC HMI WinCC flexible 2008 Communication Part 1 Hope this will helps. regards |
Last edited by: UMENCHO at: 3/16/2009 12:34 PM |
|
3/16/2009 12:36 PM | |
Posts: 30 Rating:
|
I have also a sentron pac3200 with profibus module. neither this is listed in flexible list. Is necessary to use plc?? |
3/16/2009 12:44 PM | |
Joined: 9/28/2005 Last visit: 7/24/2025 Posts: 2957 Rating:
|
If you do like UMENCHO recommends then you don't need any PLC. |
Best regards, |
|
3/17/2009 7:02 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Also if you want, you can connect this sentron pac3200 to profibus network. But the same way like ABB device. Reques GSD file. Both devices can be only profibus slave. And in your case PC will be profibus master.
Look at manual http://support.automation.siemens.com/WW/view/en/26504372 . Hope this will helps. regards |
3/23/2009 12:03 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Set PG/PC interface to CP5611(profibus). regards |
Follow us on