(0)| 1/6/2022 8:43 AM | |
|
Joined: 5/3/2018 Last visit: 2/15/2025 Posts: 56 Rating:
|
Dear All, If I buy a SIMATIC HMI TP1200 Comfort ( 6AV2124-0MC01-0AX0 ) which from the two 1. SIMATIC WinCC Professional V17 - WinCC Prof. 512 PowerTags V17 DL ( 6AV2103-0DA07-0AH5 ) or 2. SIMATIC WinCC Comfort V17 - WinCC Comfort V17 ( 6AV2101-0AA07-0AA5 ) should i try to buy? The info on these products from siemens website is not sufficient. Can someone help me with more information on the above licenses difference. Are power tags means external tags( Process tags) which are also there with WinCC Comfort V17 ( 6AV2101-0AA07-0AA5 ) like 2048 and for WinCC Prof. 512 PowerTags V17 DL (6AV2103-0DA07-0AH5 ) its 512 only. Is there any added feature difference for WinCC Prof. 512 PowerTags V17 DL. Thanks |
| 1/11/2022 1:16 PM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16658 Rating:
|
Hello check out this: https://mall.industry.siemens.com/mall/de/b1/Catalog/Products/10007458?tree=CatalogTree# there you can see the differences. Bye Murof |
Last edited by: Murof at: 01/11/2022 13:17:07If this Information really helps, you could use the Rate function |
|
Follow us on