(0)| 2/5/2022 9:16 AM | |
|
Posts: 3 Rating:
|
Hi I have a TIA project which is currently working on a PC with 22" monitor (16:9). I tried to open it on my 15" Laptop (16:9), for doing some minor modifications. Unfortunately when I start the Runtime simulation, the objects and graphics (specially the Pipes) shown compressed in comparison to my design in Wincc. I also checked the Resolution, but all the settings are Ok. The screenshots of my wincc design page and also runtime are attached. I appreciate any kind help Attachmentscreenshot.pdf (236 Downloads) |
| 2/8/2022 12:09 PM | |
|
Joined: 8/3/2009 Last visit: 1/21/2026 Posts: 16653 Rating:
|
Hello AutoGen_1042207 Try to do a compile all or a reset of the temporary files: https://support.industry.siemens.com/cs/de/en/view/109778709 Then try again. Check also if you use the same DPI settings on both Systems. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on