4/6/2009 11:47 PM | |
Posts: 133 Rating:
|
If you look at the control word chart attached normally you would have a fault resettied into P2102.This could be from a Profibus bit or areset switch wired into a binary input on the CU320. The acknowledge fault bit (r2138.7) can be BICO connected to a digital output on the CU320 which could be wired into X22.3 terminal on the 5 or 10kw SLM.
AttachmentPages from SINAMICS_S_LH1_0707_eng.pdf (503 Downloads) |
Follow us on