6/4/2022 11:18 AM | |
Joined: 8/20/2019 Last visit: 3/5/2024 Posts: 2 Rating:
|
Hi, I encountered same issue, external client unable connect to broker ( IOT2050). However, it work the other way round where iot2050 as client able connect to external broker. is there any configuration need to be set? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/07/2022 08:44:54New subject after splitting |
|
6/7/2022 10:47 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, which image are you using? Example Image or Industrial OS? For the Example Image here is the solution. Best regards! |
Last edited by: bergmanu at: 06/07/2022 11:53:34Not working for IOT2050 support anymore from March 1st, 2024. |
|
6/7/2022 11:25 AM | |
Posts: 2 Rating:
|
Hi, in order to use the MQTT client from an external PC, a listener for external IP addresses must be added to the config file: 1. open the config-file: /etc/mosquitto/mosquitto.conf 2. add the following lines to the end of the file:
3. reboot the IOT2050 To prevent unauthorised access, authentication can also be set up: https://mosquitto.org/documentation/authentication-methods/ |
Last edited by: AutoGen_3871225 at: 06/07/2022 11:36:43Last edited by: AutoGen_3871225 at: 06/07/2022 14:29:10 |
|
6/8/2022 7:20 AM | |
Joined: 8/20/2019 Last visit: 3/5/2024 Posts: 2 Rating:
|
Hi, Thanks for your guidance, my problem solved. |
This contribution was helpful to
1 thankful Users |
Follow us on