8/22/2022 1:36 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello AutoGen_374617, which PLCSIM Advanced version do you have installed? It is possible that due to a system property, the files are not recognized and the API file needs to be replaced. This can be realized via the hotfix. Here is the link to the download. S7-PLCSIM Advanced V4.0 - Correction of the V3.0 API version With best regards |
Follow us on