9/6/2022 11:43 AM | |
Joined: 11/6/2021 Last visit: 1/16/2023 Posts: 15 Rating:
|
Is there a specific procedure for Windows patching of WinCC systems (no WSUS)? I have read the links on Windows patches (Which Microsoft patches are recommended for operating SIMATIC WinCC V7 ("Security ... - ID: 18752994 - Industry Support Siemens ) But there isn't a real procedure in that link. 1. Is it necessary to Close Project and Exit Runtime? 2. Is it OK to just do the approved (excluding the non-approved) patches and just restart Windows while WinCC is running? Can there be any damage done to the SQL database if we don't Close Project and Exit Runtime? Any experiences? |
9/6/2022 1:25 PM | |
Joined: 7/19/2022 Last visit: 9/16/2025 Posts: 436 Rating:
|
Hi SergeiMalov, I recommend you to make a backup of the SQL database and then install it. Here is how to make a database backup: Under "Tag Logging > Files" you will find the database settings: https://support.industry.siemens.com/cs/ww/en/view/109760739/76673485579 You must define the backup for the database: https://support.industry.siemens.com/cs/ww/en/view/109760739/114680595467 Once it is configured, when the backups are generated, you must copy them to the "CommonArchiving" folder. In this way with the connect/disconnect backup buttons of the controls (like the curve control) you will be able to visualise the information of these curves. You can find it in the section how to connect the backup at: https://support.industry.siemens.com/cs/ww/en/view/109760739/90871533451 |
Last edited by: JBS98 at: 09/06/2022 13:27:58If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
9/6/2022 1:56 PM | |
Joined: 11/6/2021 Last visit: 1/16/2023 Posts: 15 Rating:
|
Thanks - if we are already continuously backing up the Tag and Alarm data to an external drive through WinCC Tag Management "extra backup" feature, would this suffice to comply with what you're suggesting ? And are there any other considerations? |
Last edited by: SergeiMalov at: 09/06/2022 13:57:08Last edited by: SergeiMalov at: 09/06/2022 13:58:48 |
|
Follow us on