9/28/2022 9:18 PM | |
Joined: 8/13/2018 Last visit: 8/15/2025 Posts: 2 Rating:
|
Hi everyone, I have a problem with mi IOT2050 FS 04. I installed on the emmc the image version 1.2.2. Everithing works fine when i use the UART debug, even if I unplug the USB after start. The problem is when I try start the IOT without the UART conection or specicly the Rx pin. At first, stat led goes green, and then It goes to red permanently. This is what i see at the console when uart is correctly connected: [snip] After this If I connect the Rx cable and write boot command It goes fine. Hope that someone can help me.
AttachmentConsole.txt (497 Downloads) |
Last edited by: Jen_Moderator at: 09/29/2022 05:32:55Console information as txt file added. |
|
Follow us on