10/25/2022 3:40 PM | |
Joined: 11/26/2014 Last visit: 7/12/2023 Posts: 40 Rating:
|
Hello, In my program, FB 106 "MB_CPCLI" is already occupied by FB 106 "Subnet", which is automatically generated due to the usages of I/O drivers, so I rewired the blocks hoping to resolve that issue but something seems to be wrong. Can anyone help me out, I am completely lost. I suspect some additional action is necessary, which I cannot find in the documentation. The archive of the program is attached. It includes a default and rewired version. What I did:
AttachmentSIMATIC ModbusTCP communication using CP 343-1 and CP 443-1, ModbusTCP CP V5.pdf (995 Downloads) |
Last edited by: Stefan Müller at: 10/25/2022 15:43:07Last edited by: Stefan Müller at: 10/25/2022 15:44:37Last edited by: Jen_Moderator at: 10/26/2022 07:40:07Link optimized. |
|
10/25/2022 3:45 PM | |
Joined: 11/26/2014 Last visit: 7/12/2023 Posts: 40 Rating:
|
without rewiring
AttachmentModbus_TCP_CP_default&rewired_20221025_1700_onlyProjectDefault.zip (906 Downloads) |
Last edited by: Stefan Müller at: 10/25/2022 15:59:36 |
|
10/25/2022 4:01 PM | |
Joined: 11/26/2014 Last visit: 7/12/2023 Posts: 40 Rating:
|
rewired Modbus communication noted that
are not added during compile but why? AttachmentModbus_TCP_CP_default&rewired_20221025_1700_onlyProjectRewired.zip (932 Downloads) |
10/25/2022 7:36 PM | |
Joined: 11/26/2014 Last visit: 7/12/2023 Posts: 40 Rating:
|
RTFM (assumed that Compile handles this...) adding the SIMTEC NET Library, taking the hurdle simatic-op is on a write-protected medium - Siemens - Forums.MrPLC.com, copying FC10, FC50 and FC60 solved it. |
This contribution was helpful to
1 thankful Users |
Follow us on