12/5/2022 9:17 AM | |
Joined: 9/21/2022 Last visit: 3/21/2025 Posts: 3 Rating:
|
Dear Sirs I am looking for support how to connect to CNC SINUMERIC 810T GA3 using Constant Current Adapter Type2 (https://www.ibhsoftec.com/Const-Typ2-Eng) and program S5+S7 for Windows. The technical parameters in the machine are set in accordance with the Siemens documentation I connect via the com port using the original siemens cable and the Constant Current Type 2 adapter. Unfortunately, I get an error. Could you please send me information on how to upload the PLC program correctly. Below are photos of the situation. Thank you. |
12/9/2022 3:29 AM | |
Joined: 10/17/2007 Last visit: 9/3/2025 Posts: 4429 Rating:
|
1st of all "S5+S7 for windows " is 3rd party SW--NOT Siemens. I will not support you for that--even I know that SW. Please use Siemens STEP 5 SW. 2nd--I can tell your your setting data for connect PLC programming device is GOOD 3rd--Please answer my question: do you know how to transfer DATA vis RS 232 port of 810M GA3 to/from PC/Laptop , and do you have that kind of cable?
|
If you like my comments please |
|
Follow us on