1/9/2023 8:03 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Dear AutoManiaC, as it is a S7-1200/1500 you can try to upload the project from the PLC into TIA. Indeed, there are some preconditions that must be met (like used software versions, passwords/or older S7-1200 PLC's may not support a complete upload). But in general it is worth a try. Afterwards you can make your changes and download the new hardware configuration pack into the PLC. So if the complete upload from the CPU is possible, you do not particularly need the original project. What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?regards sancruz regards sancruz |
Feedback appreciated, please rate |
|
Follow us on