1/9/2023 3:49 PM | |
Joined: 12/26/2013 Last visit: 8/30/2025 Posts: 22 Rating:
|
I want to make a simple counter in CFC. I am increasing an INT value every seconds through CPU clock memory. It was working fine. But now I want to reset that counter after 60 as like seconds in the clock. So I tried to move '0' to that value via custom made MOVE block as I coudn't fine move block. In that move block I wrote only two lines L #input T #output But after adding this block, the value of that INT value no longer increasing. It is remaining at Zero. 1. Why this is not working? 2. Is there any other way to move a constant value to Memory word? AttachmentCounter_CFC.pdf (902 Downloads) |
1/9/2023 9:02 PM | |
Joined: 9/15/2006 Last visit: 8/29/2025 Posts: 543 Rating:
|
Added the plan as PDF, as the screenshot size seems to be reduced in size to be unreadable.
Attachmentcfc-adder.pdf (835 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on