1/9/2023 9:13 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi Bruno 19, PROFINET devices usually uses multiple MAC addresses. For example see the manual "CPU 1515-2 PN": Assignment of the MAC addressesCPU 1515‑2 PN has two PROFINET interfaces, with the first interface having two ports. The PROFINET interfaces each have a MAC address, and each of the PROFINET ports has its own MAC address. The CPU 1515‑2 PN therefore has five MAC addresses in total. The MAC addresses of the PROFINET ports are needed for the LLDP protocol, for example for the neighborhood discovery function. The number range of the MAC addresses is sequential. The first and last MAC addresses are printed on the rating plate on the right side of each CPU 1515‑2 PN. Kind regards |
Follow us on