1/9/2023 9:00 PM | |
Joined: 1/21/2013 Last visit: 9/11/2025 Posts: 4102 Rating:
|
Hi GTSAGarcia, when using the OPC UA .NET stack like in the application example "Creating of OPC UA clients with .NET and helper class" it depends on the membership in the OPC foundation. For members the "RCL" model applies while for others the "GPL 2.0" model is valid. (See also the documentation of the example). Kind regards |
Follow us on