1/19/2023 6:07 AM | |
Joined: 1/21/2013 Last visit: 9/17/2025 Posts: 4111 Rating:
|
Hi kpetrov, you are looking for the EPLAN macro of a SIPLUS LOGO! 24CE. This device is based on 6ED1052-1CC08-0BA1. Use this article number to obtain the correct EPLAN macro. The download manager will always provide some downloads, even if the requested data is not available. If you are looking for a single device, I prefer to use the Industry Image Database. There you can enter an article number and you will see all available photos, graphics and CAx data. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on