10/27/2008 10:10 AM | |
Posts: 279 Rating:
|
And to answer Stuarts original question. You have a problem, because the CS and RT versions must match. In certain cases, there can be a difference in hotfix versions, a 2007 HF2 RT will work with a project made by CS 2007 HF3 for example. But major revisions must be the same, so a 2007 RT will not work withproject made by CS 2008. This is what you can do: If you have not opened the RT package, you can send it to Siemens to have it exchanged to 2008 for a fee. Or, you can purchase a 2007 to 2008 upgrade package. A more difficult approach is to use "Save as version 2007" in CS 2008. Then the saved project must be imported into CS 2007 and compiled there. I use VMware to have several versions of WinCC Flex on my PC for just this purpose. |
5/14/2009 3:41 PM | |
Joined: 1/20/2009 Last visit: 2/19/2024 Posts: 23 Rating:
|
Thanks Jesper. I have now purchased an upgrade license. I am having some trouble upgrading however since this message appears when I try to upgrade "No matching upgrade license keys were found" Anyone know why this might be? I am upgrading a 2007 runtime lisence with 2048 tags using a 2008 upgrade lisence. Thanks |
5/14/2009 4:24 PM | |
Posts: 279 Rating:
|
Hi again. Firsttransfer the upgrade license to the C: drive of the target PC. Then select the old runtime license on the C: drive, and select Upgrade. |
Follow us on