2/10/2023 1:16 PM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi Robert, there is a function called "device replacement without exchangeable medium", but therefore the topology needs to be configurend - and - also the motor must support this feature. Maybe this can help somehow. How do you replace an IO device without exchangeable medium when the topology of the PROFINET IO systems is configured?Enabling device replacement without exchangeable mediumEven if the motor is not "replaced", this function can be used to assign the device name automatically. regards sancruz |
Last edited by: sancruz at: 02/10/2023 13:18:17Feedback appreciated, please rate |
|
Follow us on