(0)| 2/17/2023 5:41 AM | |
|
Posts: 32 Rating:
|
I am working in Simatic WinCC v7.4.0 I am doing some VBS scripting to create a Excel file with multiple sheets (4 in numbers)where i can store the tags value.. Currently, i am successful in creating excel file with single sheet and writing the tag value on certain action is accomplished. Sheets.Add Count:= 4 I have also tried the method ActiveWorkbook.Sheets.Add Before:=ActiveWorkbook.Worksheets(ActiveWorkbook.Worksheets.Count) But same message keeps coming Last i tried My whole code for file creation is as mentioned below. AttachmentQuery.txt (329 Downloads) |
Last edited by: abbasisahab at: 02/17/2023 05:50:52Last edited by: abbasisahab at: 02/17/2023 05:54:22 |
|
Follow us on