3/4/2023 10:09 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Please refer below application examples, will help you. MICROMASTER 4: Function block to operate on Profibus DP MICROMASTER 4: Uploading and downloading drive parameters using STARTER MICROMASTER/SINAMICS G: Speed control of a G120/G120D/MM4 using a S7-300/400 (STEP 7 V5) with PROFINET/PROFIBUS and HMI |
Last edited by: Jen_Moderator at: 03/06/2023 10:30:02Links optimized. |
|
3/4/2023 6:52 PM | |
Joined: 4/21/2022 Last visit: 7/10/2025 Posts: 111 Rating:
|
thanks a lot but i can not dowload documents |
3/5/2023 3:22 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, You can refer G120 documents which will give you an idea. Refer Uploading and downloading drive parameters of a MICROMASTER 4xx using STARTER (1,5 MB) for communication with starter. Download parameter reading & writing of MM400 using S7-300/400 with Profibus, documents from this link. AttachmentUpload_download_MM4_parameter_using_STARTER_en.pdf (470 Downloads) |
Last edited by: Jen_Moderator at: 03/06/2023 10:32:41PDF attached from link. Link optimized. |
|
This contribution was helpful to
1 thankful Users |
Follow us on