2/13/2023 8:30 PM | |
Joined: 6/15/2021 Last visit: 8/22/2025 Posts: 8 Rating:
|
After some digging; 1. I found the post below that pretty well showcases what I'm looking for. The only issue with this solution is that it requires stopping runtime and going into commissioning settings. This isn't an ideal user experience but could work if there's no other option. How do you change the connection from the operator panel to the controller? 2. I see there is a "ChangeConnection" function for HMI buttons. On paper this does what I want but I am having trouble configuring it. I see that since TIA V11 it is not possible on an S7 1200? The post mentioning that is from 2017 so hopefully this has been fixed. Any insight would be appreciated |
Follow us on