5/22/2009 12:23 PM | |
Posts: 22 Rating:
|
Hello, i'm trying to make a selftune in one machine with four heating zones, I have read all documentation, and I don't understand one value : TUN_DLMN. Some one can explain the function of that value? At the end of tunning, happens a overshot and the information code 20020, and I think has some to have with that value, but I don't know what for, so I can't ajust it corretly. One more thing, some one can give the corretly order for tuning? My way is, select e low setpoint (ex: 30º) and then when temperature get stabe, I turn on TUN_ON and wait 1min, then select a hight setpoint (like 120º), then temperatura raises and near 120º all tunes stop and give information 111 (like phase 7 is ok) and 20020 (like point of inflection not reached) And I don't know what to do.. Thaks, Luis Lourenço AttachmentEnsaio_T.zip (368 Downloads) |
Last edited by: Dotinho at: 5/22/2009 12:23 PMIn Attachment is the project. |
|
5/22/2009 3:01 PM | |
Posts: 22 Rating:
|
Sorry, I have understand that. the value is the total power percentage during tuning.. Thanks |
This contribution was helpful to
1 thankful Users |
Follow us on