5/19/2009 10:01 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, i found this Infos. Maybe this could be helpful. -> http://support.automation.siemens.com/WW/view/en/26283062 -> http://support.automation.siemens.com/WW/view/en/24677043 regards, |
5/20/2009 1:41 PM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi You can read out the SQL database which isdescribed inthe following entry: http://support.automation.siemens.com/WW/view/en/26283062 Maybe you can use local tags to add the datain your own control. Bye |
Last edited by: ZAK at: 5/20/2009 2:21 PMwrong website |
|
5/26/2009 1:01 AM | |
Posts: 279 Rating:
|
Hi sbiughy. I also went looking for a grid activex that will work with WinCC Flex. The only one that seemed to work was this one: http://www.bogemic.com/grid-activex-control-overview.php In the end I found it to have far too many functions for my need (I prefer small and simple), so I didnt actually go and use it for real. Not sure how reliable it is as I didnt work with it in depth. Let me hear how it goes. I am still interested in a simple Grid object for Flexible. There ought to be one built-in already. |
5/26/2009 9:49 AM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi If you have installed MS Excel than you can use theActiveX object "Microsoft Office Spreadsheet 11.0". You find an example in the following FAQ (Attachment 2): http://support.automation.siemens.com/WW/view/en/24327008 The FAQdescribes the option Audit of WinCC flexible but in the attachment 2 isan example with these ActiveX Control. Bye |
Follow us on