(0)| 5/4/2023 7:57 AM | |
|
Joined: 7/19/2022 Last visit: 1/20/2026 Posts: 436 Rating:
|
Hello LucasFWB, I think you can do it if you follow the following steps: 1. Create a button to export data to SD card. 2. Loads but without overwriting, this is important to not lose what you have in the RT. 3. Export the data (.csv) to the SD from the button created. 4. Load that .csv to the engineering project and load the recipes again.
|
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
| 5/5/2023 11:53 AM | |
|
Joined: 8/3/2009 Last visit: 1/23/2026 Posts: 16661 Rating:
|
Hello Yes this steps are also explained in this FAQ: http://support.automation.siemens.com/WW/view/en/98784532 -> Of course you do not want to migrate but the steps are basically the same you can also export to csv, then edit the datarecords in a csveditor or notepad and then import in the runtime again. If you run the Diagnose Webpages on the TP then you can also access to it with webbrowser from outside and eyport without having buttons in Runtime. Bey Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on