5/30/2023 9:45 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, If the preconditions are met, it is possible to upload the program from the cpu. If it is an "older" S7-1200, there may be limitations, some older CPUs does not support the complete upload including hw-config. What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
Follow us on