6/6/2023 1:59 PM | |
Joined: 3/28/2023 Last visit: 12/2/2024 Posts: 3 Rating:
|
Regarding the upload, this problem should not exist, right? I'm trying to upload a PLC 1214C DC/DC/DC with firmware V4.5 programmed in Tia Portal V15.1, to a blank program in the same Tia Portal v15.1, but an error is happening! In the Tia Portal v15.1 catalog there is no firmware version 4.5 for this PLC. Attached error image. ------------------------------------------------------------------------------------------ |
Last edited by: diassbruno at: 06/06/2023 14:00:35Last edited by: diassbruno at: 06/06/2023 14:08:34Last edited by: Jen_Moderator at: 06/07/2023 08:35:23New subject after splitting |
|
6/7/2023 9:48 AM | |
Joined: 3/30/2020 Last visit: 9/2/2025 Posts: 5416 Rating:
|
The software should not crash like that - regardless of what the CPU firmware is. Attempt to connect to the PLC via "online access". Check the online information of the PLC. One of the entries there would say which software was used to load to it. The latest highest firmware that Step7 V15.1 can handle is V4.3. But it needs an HSP (hardware service pack) to be loaded. That might be your problem. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
6/7/2023 1:24 PM | |
Joined: 3/28/2023 Last visit: 12/2/2024 Posts: 3 Rating:
|
Hello qwazee, problem solved! I was able to upload the program, but not with a blank program. In the company's database there is the old program for the equipment, I accessed the PLC with this old program and uploaded it overwriting the data, in this way I was able to monitor the equipment without causing the error.
|
This contribution was helpful to
2 thankful Users |
Follow us on