5/29/2009 12:07 PM | |
Posts: 52 Rating:
|
hello to all I have a problem connecting a MP377 multipanel to a HP 6980 inject printer I follow the connection settings I found on this link http://support.automation.siemens.com/WW/view/en/11376409 but when i start the runtime again and try to print something . I get the following message "Not Standard Printer. Error 10001" I have check that the printer can print. I have check the cable , what else should we check? Is there a possibility that the firmware on the panel is wrong? |
Last edited by: StavrosGR at: 5/29/2009 12:07 PM |
|
5/29/2009 12:43 PM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi Maybe you use the wrong printer settings. Link to the FAQ: http://support.automation.siemens.com/WW/view/en/14668901 Bye |
5/29/2009 12:59 PM | |
Posts: 52 Rating:
|
No the Printer Language is set on PCL Inject, and the port is set to USB. |
Follow us on