(1)| 7/3/2023 9:38 AM | |
|
Posts: 304 Rating:
|
Hi! Could you share with us the version that you are using? Br! |
| 7/4/2023 6:12 AM | |
|
Joined: 11/4/2021 Last visit: 12/9/2024 Posts: 8 Rating:
|
I tried with V17 update 6 and V18 update 1 In the MTP700 I tried Operating system 16 and 18 Now the situation is like in the photos Thanks AttachmentUnified.pdf (470 Downloads) |
| 7/10/2023 5:32 AM | |
|
Joined: 11/4/2021 Last visit: 12/9/2024 Posts: 8 Rating:
|
Any update ? Thanks |
| 7/11/2023 5:23 AM | |
|
Joined: 1/21/2013 Last visit: 1/22/2026 Posts: 4427 Rating:
|
Hi daniele.gemignani, It would help us to know exactly what you are struggling with. You are referring to video timestamp 0:45. This is where the VLC media player shows the available audio devices. Your screenshot only shows the default devices. This would indicate that you have not connected a supported audio device. The "cards" file shown at 4:32 will always contain "PCH" and "pcsp". If there is a 3rd entry, use it. You should be aware that the device names depend on the hardware you are using. I tested with a Sennheiser PC 8 USB and for that headset the card is named "headset". Kind regards |
Follow us on