(1)| 8/14/2023 4:33 PM | |
|
Joined: 11/8/2017 Last visit: 1/16/2026 Posts: 361 Rating:
|
Hi, I can't comment on the Zennio display that you are using, but it sounds like you want to setup a Master/Slave configuration with your DXRs. You will of course need to connect the DXRs together via IP. For Master/Slave operation - in your case, your display is connected to the 'Master' DXR, and the 3x 'Slave' DXRs mimic the operation of the Master DXR, i.e. all Slaves follow what the Master is doing. To configure this in ABT, see attached. You need to drag and drop the room segments associated with the Slave DXRs into the Master DXR. Once this is done, you will need to download the changes into all of your DXRs. Regards, AttachmentMasterSlave.zip (478 Downloads) |
Last edited by: CJ. at: 08/14/2023 16:40:15 |
|
This contribution was helpful to
|
|
Follow us on