9/29/2023 12:35 PM | |
Joined: 7/11/2022 Last visit: 8/25/2025 Posts: 56 Rating:
|
Hello, Upon clicking two radio buttons, I intend to dynamically add a trend to an Online Trend Control in Siemens WinCC V8.0. The text extracted from the button tooltips will serve as the name for the archived tag value which will be displayed. My code is in description. "ValueX" and "ValueY" are internal text tags. Problem is that I can't delete previously selected trend, or operations with chars are not valid. Help is more than welcomed. AttachmentSTRNCAT.TXT (240 Downloads) |
10/2/2023 7:26 AM | |
Joined: 7/11/2022 Last visit: 8/25/2025 Posts: 56 Rating:
|
Thank you for your answer, however this code attached in the file blocks me from working in the runtime and returns a large number of errors after which I cannot close the runtime normally. What can be the problem if the debugger does not recognize the error?
AttachmentForumScript.txt (244 Downloads) |
Follow us on