(0)| 10/12/2023 7:43 AM | |
|
Posts: 8 Rating:
|
Hello everyone, Im try to connect Multiple light beam safety device (MLD510-RT3/A) Asi interface to PLC S7-1200. I use AS-i Master CM 1243-2 and AS-i Data Decoupling Unit DCM 1271 to connect this device. Because Multiple light beam safety device (MLD510-RT3/A) factory slave address =0. To configure i want to change slave address to =1. I want to ask if TIA PORTAL can set the slave address for ASi-Slave Device. Many thanks for any idea, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2023 12:55:10New subject after splitting |
|
| 10/12/2023 12:55 PM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Connect MLD510-RT3/A Asi interface to PLC S7-1200 is published within the conference Communication / Networks. Jen_Moderator |
Follow us on