(0)| 10/19/2023 3:33 PM | |
|
Joined: 3/30/2020 Last visit: 1/21/2026 Posts: 5668 Rating:
|
Hello. It is only possible to upgrade the software version if you have an offline project. For your case you will need Step7 V14 to upload the program from the PLC to the PC. Then the uploaded project can be converted to V18. Installing Step7 V14 on a PC that has Step7 V18 is possible. Running Step7 V18 with the license of Step7 V18 is also possible. Unfortunately the installation files are not available on Siemens' site anymore. So if you want Step7 V14 install files, you will need to contact Siemens. You can use the "Support Request" link. Official information: [LINK: What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?] ~ |
|
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
|
|
Follow us on