(0)| 10/27/2023 7:18 AM | |
|
Posts: 1 Rating:
|
Hello , I am facing problem in WinCC 7.5 startup at windows 11 home . Error showing as " Can not open WinCC project - Project manager configured server is not running. Check the computer name of the server. " to resolve the problem we have installed WinCC 7.5 sp2 on this . but problem remaining same . So anyone pls help me how we resolve the problem. Regards VSingh ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/27/2023 10:43:09New subject after splitting |
|
| 10/27/2023 11:48 AM | |
|
Joined: 2/17/2020 Last visit: 1/21/2026 Posts: 1251 Rating:
|
Hi, I believe Windows 11 Home is not released for WinCC V8, so I would recommend following this FAQs but could not guarantee it will work as the operating system is not compatible with the software: Update configuration file of the WinCC project (delete DCF) What options does the WinCC Project Duplicator provide for creating a redundant server project? Note: When the project is closed, the ProjectDuplicator "Save as..." option can be used. It may also be necessary to restart the computer before copying the project. Hope that helps. |
|
A rating will be well appreciated. |
|
Follow us on