(1)| 11/12/2023 1:25 AM | |
|
Joined: 8/19/2022 Last visit: 11/28/2025 Posts: 3 Rating:
|
Hi, I'm new to WinCC Unified. Maybe the following could help. I wanted to show the active recipe written to the PLC when user click the "Write To PLC" button from the UI parameter set control. With a parameter set control there are two (2) actions needs to be done. Also, three (3) internal tags are required. 1- As indicated in this thread, the ID can be extract by adding a script to the "current parameter set id" of the control. 2- In the "Events" of the same parameter set control, add a script to "Command fired". There are some magic numbers. If an enum exists for those, I was unable to find them. ------------------------------------------------------------------------------------------ |
Last edited by: RichardIndustrialControl at: 11/12/2023 01:41:06Last edited by: RichardIndustrialControl at: 11/12/2023 01:43:14Last edited by: RichardIndustrialControl at: 11/12/2023 01:43:48Last edited by: RichardIndustrialControl at: 11/12/2023 01:53:30Last edited by: Jen_Moderator at: 11/13/2023 11:07:05New subject after splitting |
|
Follow us on