1/3/2024 7:25 AM | |
Joined: 11/29/2018 Last visit: 3/4/2025 Posts: 4 Rating:
|
Thanks Denilson for this post. How is possible to use local tag for index of array. I would like to create one page for analog settings (a lot of analog signals). In a simple configuration with one hmi and one plc i can use in plc a db of array and use an internal tag hmi for index. But if we have a unified runtime pc and i want to use also 2 or 3 client, i don't know how make independent the client with the array. is not possibile to use the local tag as index tag of an array in the hmi tags. The only solution at the moment for me is to create one page for every analog signal but it is a lot of work. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/03/2024 12:05:40New subject after splitting |
|
Follow us on