7/7/2023 7:28 AM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi Schnitze, So at first glance, it may be a bug since it sounds to me that this ID has been reported on some occasion to the Siemens development department. Anyway, could you tell us the OS version of the device including the build and the TIA Portal version with which you have created the project? Also a capture of the alarm that you indicate in case I could find some more information. Best regards!
|
If this Information really helps, you could use the Rate function |
|
7/7/2023 2:10 PM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi Schnitze, I would recommend that you try updating the TIA Portal to the latest released version, recompiling and uploading the project to the panel again. To see if any of the updates fix this system alarm. "Updates for STEP 7 V18, S7-PLCSIM V18 and WinCC V18" If after doing this it still happens, I would create an SR to the Siemens technical service so that they report it to development since it is most likely a bug. In this way, they will be able to see that it is an issue that they must resolve. Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on