2/16/2017 2:24 PM | |
Posts: 6 Rating:
|
Hello thank you for your answer Could you give me the steps to solve this problem. It is my first time using sinumerik |
2/16/2017 7:02 PM | |
Posts: 6 Rating:
|
Hello again Added to the error below, Even when I press by the reset button, the led associated with Feed Stop stays on. Have you any idea and what can I do ?
|
2/17/2017 6:02 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello ahmed89, NC will complete the process of reading values of leading & synchronisation axis as well as referencing & when the difference between leading & synchronisation axes is less than value set in MD 37110 i.e. GANTRY POS TOL VALUE, gantry grouping is synchrinized is set to 1 & gantry axes are re-activated i.e. recoupled. The message displayed "Channel 1 synchronisation of gantry group 1 is in progress" is standard & not warning or alarm. This is displayed at power ON condition when NC activates gantry group axis. Please check spindle & feed On keys status, must be ON & feed selector switch must not be at 0. HTH.
|
This contribution was helpful to
1 thankful Users |
Follow us on